Accueil » Blog » Soutien à la conception : du développement à la production

Soutien à la conception : du développement à la production

Les capacités de soutien à la conception de Boyd sont réparties sur une variété de technologies pour répondre aux besoins d’une variété d’industries. En tant que fabricant sur mesure, Boyd doit être prêt à répondre à un large éventail de besoins d’un client. Our specialties lie in thermal, mechanical, industrial, manufacturing, graphic, and electrical design support, providing design considerations for manufacturability and managing projects in a coordinated, efficient manner to meet the agreed requirements of a project.

Boyd Supports Your Complex Projects

When supporting a customer's project, Boyd engages multiple departments to review designs. This in-house product development team includes product line managers, the rapid prototyping group, design engineers, and the process engineering group. Boyd's development team is adept at supporting everything from our customers' complex projects with demanding requirements to more straightforward components where customers only engage our manufacturing expertise. Adept customers leverage Boyd's wholistic design view, where we seek to integrate functionality and simplify assembly and BOMs for a cost saving, multifunctional component.

Manufacturing and Material Science Expertise

In addition to developing a design, we ca also develop the manufacturing process. Custom part production require efficient, reliable, and repeatable manufacturing processes. Boyd excels at innovating and refining new and existing processes to push the boundaries of current manufacturing capabilities. The process begins by obtaining requirements from the customer with sufficient detail and specification such as thermal management, moisture ingress, UV, chemical, or corrosion resistance, etc.. Then, we help create a development plan with assigned roles and timelines. Next, validation parts are fabricated, tested, revised, and validated before starting production.

Vertical Integration, Decreased Costs

Boyd is a vertically integrated manufacturer that offers a wide range of in-house value-added capabilities and services. To further simplify your supply chain, we source high quality materials from our extensive network of strategic partners and suppliers to ensure that we provide our customers with an exceptional product.

Vertical Integration, Decreased Costs

Quality is key in manufacturing, and Boyd is compliant to internationally recognized quality standards across several industries including mobile, aerospace, and medical. Although quality standards are specific to each facility, a few certifications maintained by Boyd include: ISO 9001, IATF 16949, ISO 14001, ISO 13485:2016, and AS9100. To learn more about our certifications, check out our quality and compliance page.

Our company has multiple facilities throughout the US, Europe, and Asia and leverage our global capabilities to produce advanced integrated solutions where our customers need them. If you would like more information about our processes and development capabilities for your company’s next product, please contact us to request a consultation with one of our in-house technical experts.

Articles connexes

Qu’est-ce que les dispositifs CGM ?

Qu’est-ce que les dispositifs CGM ?

Qu’est-ce que les dispositifs de surveillance continue de la glycémie ? Les dispositifs de surveillance continue du glucose (CGM) sont de petits appareils médicaux portables...

Qu’est-ce que le NVH et le BSR

Qu’est-ce que le NVH et le BSR

Introduction au NVH et au BSR Le bruit, les vibrations et la rudesse (NVH) sont des caractéristiques indésirables dans un système mécanique....

Vous aimerez aussi

Qu’est-ce que les dispositifs CGM ?

Qu’est-ce que les dispositifs de surveillance continue de la glycémie ? Les dispositifs de surveillance continue du glucose (CGM) sont de petits appareils médicaux portables...

Qu’est-ce que le NVH et le BSR

Introduction au NVH et au BSR Le bruit, les vibrations et la rudesse (NVH) sont des caractéristiques indésirables dans un système mécanique....

Vous avez des questions ? Nous sommes prêts à vous aider !